earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
功能: 时间表
产品版本: 2024, 7.0
2024/12/3

Adding a Weekly Event

You add weekly events to a schedule to determine when the event is to regularly occur. Weekly events always occur regularly unless overridden by an exception event.

显示更多
action_close

A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.

 
action_zoom_plus_stroke Weekly events in an EcoStruxure Building Operation schedule
图: Weekly events in an EcoStruxure Building Operation schedule

If there are any non-routine events, such as holidays, you can use exception events to override the schedule. 有关更多信息,请参阅 Exception Events in WorkStation .

To add a weekly event
  1. In WorkStation, in the System Tree pane, select the schedule you want to add the weekly event to.

  2. Click the Basic tab.

  3. On the Basic Schedule Editor toolbar, click the View weekly schedule events button

     
    action_zoom_plus_stroke
    .

  4. In the grid, click the start time. Drag the cursor vertically to select the end time and then horizontally to select all days for which the event should be valid.

  5. On the File menu, click Save .

  • Adding a Calendar Exception Event
  • Adding a Date Exception Event
  • Adding a Date Range Exception Event
  • Adding a Calculated Exception Event
  • Basic View of the Schedule Editor
  • Weekly Events in WorkStation
  • Schedule Events