The Advanced view of the Schedule Editor has the features of the Basic view with some additional capabilities. All the tasks that you can perform in the Basic view, you can also perform in the Advanced view.
Unlike the Basic view, the Advanced view lists the exception and weekly events in an event tree. In addition, there is a Combined option that displays all the weekly and exception events for a selected date.
Two toggles provide additional options:
Mode : Switches between an editor or preview mode.
View : Switches between a graphical or text view.
The Mode toggle provides the following capabilities:
Editor mode where you can view or edit a weekly event or an exception event.
Preview mode where you can preview (but not edit) all the weekly schedules and exceptions for a selected date. However, only the effective weekly and exception events display for that date. Typically, you see one weekly and one exception event.
Graphic View where you can view or edit a weekly event or an exception event. Para obtener más información, consulte Modifying a Schedule Using the Graphic View .
Text View where you can define specific time sequences or to break down a time value into hundredths of a second. Para obtener más información, consulte Modifying a Schedule Using the Text View .
You can view all of the events for a selected date using both the Combined option and Preview mode. Events can include exception and weekly events, and the Default value. You can toggle the combined events between the Graphic View or Text View .
Para obtener más información, consulte Advanced Schedule Editor Toolbar .