Funzionalità: Programmi orari
Versione del prodotto: 2023
17/12/2022

Advanced View of the Schedule Editor

arrow1_rotationMode arrow1_rotationView arrow1_rotationCombined

The Advanced view of the Schedule Editor has the features of the Basic view with some additional capabilities. All the tasks that you can perform in the Basic view, you can also perform in the Advanced view.

Unlike the Basic view, the Advanced view lists the exception and weekly events in an event tree. In addition, there is a Combined option that displays all the weekly and exception events for a selected date.

Two toggles provide additional options:

  • Mode : Switches between an editor or preview mode.

  • View : Switches between a graphical or text view.

 
action_zoom_plus_stroke Advanced view of the Schedule Editor
Figura: Advanced view of the Schedule Editor

Mode

The Mode toggle provides the following capabilities:

  • Edit Schedule mode where you can view or edit a weekly event or an exception event.

  • Preview Events for Selected Date mode where you can preview (but not edit) all the weekly schedules and exceptions for a selected date. However, only the effective weekly and exception events display for that date. Typically, you see one weekly and one exception event.

View

The View toggle provides the following capabilities:

 
action_zoom_plus_stroke Text View
Figura: Text View

Combined

You can view all of the events for a selected date using both the Combined option and Preview Events for Selected Date mode. Events can include exception and weekly events, and the Default value. You can toggle the combined events between the Graphic View or Text View .

 
action_zoom_plus_stroke Combined Events in Graphic View
Figura: Combined Events in Graphic View
 
action_zoom_plus_stroke Combined Events in Text View
Figura: Combined Events in Text View

Per maggior informazioni, consulta Advanced Schedule Editor Toolbar .

  • Schedule Editor Overview
  • Eventi del programma orario
  • Tipi di programma orario
  • Priorities
  • Advanced Schedule Editor – Graphic View
  • Advanced Schedule Editor Toolbar
  • Modifying a Schedule Using the Text View
  • Modifying a Schedule Using the Graphic View