Use the Basic tab to enable the archiving function, set delay, and select the format of the archive file.
Component |
Description |
Enabled |
Select True to activate the archiving function. |
Path |
Type the path to the location where you want to create your archive. |
IsValidPath |
Select True to indicate the objects have passed the validation. |
Output format |
Select the output format of the archive. For more information, see Archiving Formats and Storage . |