earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2023
2022/12/16

Assignment Properties

Use the Assignment properties to configure which user or user group receives the assignment request.

 
action_zoom_plus_stroke Assignment properties
图: Assignment properties

表格: Assignment Properties

Component

Description

Status

Select Disabled to deactivate the assignment function.

​Schedule

Enter the schedule or other multistate variable that contains the value that is to be used to activate the assignment.

Active value

Enter the value, generated by the connected schedule or other multistate variable, that is to activate this assignment object.

Assigned to

Click the browse button to open the Users and Groups dialog box where you select the EcoStruxure Building Operation user or user group to receive the assignment request. 有关更多信息,请参阅 Users and Groups Dialog Box .

  • Alarm Control Panel Objects in Multiple Servers
  • User Cannot Be Assigned to an Alarm
  • General Information Properties – Basic Tab
  • Users and Groups Dialog Box