earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Schedules
Product version: 2023
12/17/2022

Basic View of the Schedule Editor

The Basic view of the Schedule Editor serves as a workspace to plan and design a schedule. You use this editor to create, manage, and display weekly scheduled events and exception events.

You can also display the client time zone and the server time zone in the Basic view. This is convenient if your EcoStruxure BMS server is located in a time zone that is different from the time zone where you are configuring the schedule. For more information, see Time Zones .

The following figure displays the schedule of the lights within the building. The weekly events are in green and the exception event in blue. The values of the events are also displayed. Monday, November 12 is an exception event so it does not follow the same scheduled events as the rest of the week. The lights are off all day. For the rest of the week, the lights turn on at 07:00 and turn off at 18:00.

 
action_zoom_plus_stroke Basic view of the Schedule Editor
Figure: Basic view of the Schedule Editor
  • Schedule Editor Overview
  • Advanced View of the Schedule Editor
  • Time Zones
  • Schedule Colors in WorkStation
  • Schedule Editor ​– Basic View
  • Basic Schedule Editor Toolbar