earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Schedules
Product version: 2023
12/17/2022

Schedule Editor Overview

You use the Schedule Editor to create and manage schedule events for digital, multistate, and analog schedules. The schedule events that you create can be weekly events or exception events. A weekly event recurs on a weekly basis. An exception event defines either a one-time change or a recurring change that overrides the standard weekly events. In the Schedule Editor, you can view the schedule events in Basic view or Advanced view.

Basic View of the Schedule Editor​

The Basic view of the Schedule Editor serves as a workspace to plan and design a schedule. You use this editor to create, manage, and display weekly scheduled events and exception events.

For more information, see Basic View of the Schedule Editor .

Advanced View of the Schedule Editor

The Advanced view of the Schedule Editor has the features of the Basic view with some additional capabilities. All the tasks that you can perform in the Basic view, you can also perform in the Advanced view.

For more information, see Advanced View of the Schedule Editor .

Schedule Colors

A schedule has a color code so you can identify weekly events and exception events at a glance. This color code can assist you when you are modifying your schedule or trying to troubleshoot any problems.

For more information, see Schedule Colors in WorkStation .

  • Schedules Overview
  • Schedule Editor ​– Basic View
  • Advanced View of the Schedule Editor
  • Schedule Colors in WorkStation