earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Schedules
Product version: 1.8, 1.9
1/31/2012

Editing the Start Time for a Schedule Event

You edit the start time for a schedule event to make the event start at another point of time in the schedule. You can edit the start time for weekly events and single date exception events.

Show More
action_close

A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.

For example, in an analog schedule, for Monday, you schedule an air vent in a gym to open to 40 % at 08:00 for a yoga class. For a more intense class at 10:00, you schedule the air vent to open to 100 % until 13:00. Finally, at 13:00, you schedule the air vent to close to 60 % until 20:00.

 
action_zoom_plus_stroke Example weekly events for a Monday
Figure: Example weekly events for a Monday

These events occur every Monday unless an exception event overrides the weekly event.

To edit the start time for a schedule event
  1. In WebStation, in the System Tree pane, select the schedule with the event you want to edit.

  2. Navigate to the schedule event you want edit.

  3. Point to the upper border of the event, and when the pointer shape changes to a four-headed arrow, drag the whole event up, down, right, or left to the new start time in the schedule.

    Note:

    To help you avoid mistakes, WebStation warns you when you make changes in a schedule or calendar for today’s date.

  • Weekly Events in WebStation
  • Exception Events in WebStation
  • Schedule Workspace Toolbar
  • Schedule Editor in WebStation
  • Editing the End Time for a Schedule Event
  • Editing a Weekly Event
  • Editing a Date Exception Event
  • Schedule Workspace