earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Schedules
Product version: 1.8, 1.9
2/13/2014

Editing a Weekly Event

You edit a weekly event to change the information about a weekly event on a single day.

Show More
action_close

A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.

For example, in an analog schedule, for Monday, you schedule an air vent in a gym to open to 40 % at 08:00 for a yoga class. For a more intense class at 10:00, you schedule the air vent to open to 100 % until 13:00. Finally, at 13:00, you schedule the air vent to close to 60 % until 20:00.

 
action_zoom_plus_stroke Example weekly events for a Monday
Figure: Example weekly events for a Monday

These events occur every Monday unless an exception event overrides the weekly event.

To edit a weekly event
  1. In WebStation, in the System Tree pane, select the schedule you want to edit.

  2. In the Schedule workspace, navigate to the event you want to edit.

     
    action_zoom_plus_stroke
  3. In the Event grid, click the weekly event you want to edit.

  4. Edit the properties.

     
    action_zoom_plus_stroke

    Table: Schedule Event Properties Dialog Box – Weekly View

    Component

    Description

    Event type

    Click Weekly to select a weekly event type.

    All Day

    Select All Day for an all day event.

    Start time

    Double-click and type a start time for the exception event.

    End time

    Double-click and type an end time for the exception event.

    Value

    Double-click and type a value for the exception event.

  5. Click Update .

    Note:

    To help you avoid mistakes, WebStation warns you when you make changes in a schedule or calendar for today’s date.

  • Weekly Events in WebStation
  • Exception Events in WebStation
  • Schedule Editor in WebStation
  • Schedule Workspace Toolbar
  • Schedule Workspace
  • Schedule Event Properties Dialog Box – Weekly View
  • Adding a Weekly Event
  • Editing the Start Time for a Schedule Event
  • Editing the End Time for a Schedule Event