Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Programaciones
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Creating a Digital Schedule

You create a digital schedule to control the state of a digital value.

Mostrar más
action_close

A digital schedule controls a device that has an on output state and an off output state.

For example, you can create a digital weekly schedule that is bound to a digital output, such as a light switch. To turn on the lights Monday through Friday from 08:00 to 17:00, you can set the value to On when the schedule is active and Off when the schedule is inactive.

 
action_zoom_plus_stroke Digital Schedule
Figura: Digital Schedule

To create a digital schedule
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server or the folder where you want to create the schedule.

  2. On the File menu, point to New and then click Schedule .

  3. In the Create Object wizard, in the object type list, select Digital Schedule .

  4. In the Name box, type a name for the schedule.

  5. In the Description box, type a description for the schedule.

  6. Click Create .

Now you can add events to the digital schedule and bind it to a digital value.

  • Adding a Weekly Event
  • Create Object Dialog – Naming the Object Page
  • Binding a Digital Value to a Digital Schedule
  • Adding a Calendar Exception Event
  • Cómo añadir un evento de excepción de calendario
  • Adding a Date Range Exception Event
  • Adding a Calculated Exception Event
  • Digital Schedules
  • Schedule Types
  • Create Object Dialog – Naming the Object Page