earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Trends
Product version: 1.9
10/12/2017

Creating a Meter Trend Log

You use the meter trend log to record the value of a meter and seamlessly handle consumption calculations independent of meter rollover and meter exchange.

Show More
action_close

​The meter trend log is a variable triggered trend log with extra functionality to seamlessly handle consumption calculations independent of meter rollover or meter exchange.

For more information, see Variable Triggered Trend Logs .

You create and configure meter trend logs using WorkStation.

For example, in the figure below, the meter trend log records a meter the 1st of every month. In the middle of February the meter rolls over to 00000. A chart with meter consumption calculation prints the consumption every month.

 
action_zoom_plus_stroke Meter trend log
Figure: Meter trend log

When physically replacing an old meter with a new one, you have to configure the meter trend log by adding the settings of the old meter and new meter in the Manage replacement of meter dialog box in WorkStation. These settings are the foundation to handle a meter rollover or calculating consumption though meter replacement. For more information, see Manage Replacement of Meter Dialog Box .

 
action_zoom_plus_stroke Manage replacement of meter dialog box where you enter the values of the new and old meter.
Figure: Manage replacement of meter dialog box where you enter the values of the new and old meter.
Note:
  • In order for a meter rollover to be managed correctly in the meter trend log and to ensure logging starts at the correct energy reading value, you enter previous meter and new meter information in the Manage replacement of meter dialog box. For more information, see Managing Replacement of a Meter .

To create a meter trend log
  1. In WorkStation, in the System Tree pane, select the folder or SmartStruxure server where you want to create the trend log.

  2. On the File menu, point to New , and then click Trend .

  3. Select Meter Trend Log .

     
    action_zoom_plus_stroke
  4. In the Name box, type a name for the trend log.

  5. In the Description box, type a description.

  6. Click Next .

  7. In the Logged variable box, enter the variable that you want to log.

     
    action_zoom_plus_stroke
  8. Click the Set unit button

     
    action_zoom_plus_stroke
    .

  9. Select a unit for the trend log values.

     
    action_zoom_plus_stroke
  10. In the Prefix box, select the prefix of the unit.

  11. Click Select .

  12. In the Delta box, enter the minimum value change that triggers a new record.

  13. In the Trigger variable box, enter the variable that triggers the log.

  14. In the Trigger condition box, select when to record the value of the logged variable.

    • Select Change to true to record the value of the logged variable when the trigger variable changes to true.

    • Select Change to false to record the value of the logged variable when the trigger variable changes to false.

    • Select All changes to record the the value of the logged variable anytime the trigger variable changes state.

  15. In the Log size box, select the number of records to be recorded before old ones are overwritten.

  16. In the Available trend storage box, check that the available number of records is not exceeded.

  17. In the Clear when enabled box, select True to clear the trend log every time the trend log is enabled.

  18. Click Next .

  19. In the Start time box, enter the time when the meter is installed.

     
    action_zoom_plus_stroke
  20. In the Start value box, enter the value of the meter when it was installed.

  21. In the Meter constant box, enter the constant of the meter.

  22. In the Min value box, enter the first value of the meter when it rolls over.

  23. In the Max value box, enter the last value of the meter before it rolls over.

  24. Click Next .

  25. In the Extended Trend Log box, click the Browse button

     
    action_zoom_plus_stroke
    to create an extended trend log and connect it to the trend log.

     
    action_zoom_plus_stroke
  26. In the Trend Log List box, click the Browse button

     
    action_zoom_plus_stroke
    to create a trend log list and connect it to the trend log.

  27. In the Trend Chart box, click the Browse button

     
    action_zoom_plus_stroke
    to either create a new trend chart or connect the trend log to an existing trend chart.

  28. Click Create .

The meter trend log is created in the selected folder.

Note:
  • When a meter trend log is created, you need to add the current meter value.

  • Meter Trend Logs
  • Managing Replacement of a Meter
  • Trend Units
  • Log Record Storage
  • Create Object Wizard – Naming the Object Page
  • Create Trend Log Wizard – Configure Meter Trend Log Page
  • Creating an Extended Trend Log
  • Creating a Trend Log List
  • Creating a Trend Chart that Monitors a Trend Log Series
  • Trend Log Wizard – Initial Meter Settings Page