earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: WebReports
Funktionaliteter: Rapporter
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021-12-16

Creating a Prompted Report in WebReports

You create a prompted report when you want a report that prompts for filtering criteria before the report is generated.

Visa mer
action_close

A prompted report is a report that processes user-specified filtering criteria to generate the report output. With prompted reports, you enter and select filtering criteria for one or more input parameters, and then run the report. The generated report output provides information that is based on your filtering criteria.

In WebReports, some prompted reports are factory supplied reports provided by Schneider Electric. You receive these reports when you install WebReports, and can view these reports in both WorkStation and your Web browser. Mer information finns i Factory Supplied Reports .

Other prompted reports are custom reports that you can create using the WebReports features in both WorkStation and your Web browser. Mer information finns i Custom Reports .

To generate and view a prompted report in WorkStation, you select the report in the Reports folder in the System Tree pane.

 
action_zoom_plus_stroke Prompted Report in the System Tree pane
Figur: Prompted Report in the System Tree pane
 
action_zoom_plus_stroke Prompted report output in WorkStation
Figur: Prompted report output in WorkStation

When you select the report, the input parameters display in the Work area so you can enter your filtering criteria. After you click Run report, the report output displays in the Work area.

To generate and view a prompted report in your Web browser, you log on to the WebReports Web site, and then select the report in the Reports Tree.

 
action_zoom_plus_stroke Prompted report in the Reports Tree
Figur: Prompted report in the Reports Tree
 
action_zoom_plus_stroke Prompted report output in a browser
Figur: Prompted report output in a browser

When you select the report, the input parameters display in your browser so you can enter your filtering criteria. After you click Run report, the report output displays in your browser.

To create a prompted report in WebReports
  1. In WebReports, on the menu bar, click View .

  2. In the Reports Tree , select a prompted report, such as a production report.

  3. Enter the filtering criteria for the report.

  4. Click Submit Form .

  5. Click Save as .

  6. In the Report name box, type a folder name and report name for the custom report.

  7. Clear the Dashboard report box.

  8. Click Save as .

  • Prompted Reports
  • WebReports Main Page
  • Creating a Prompted Report in WorkStation
  • Viewing a Prompted Report in WorkStation
  • Viewing a Prompted Report in WebReports