earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: WebStation
Funktionaliteter: Användarhantering
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2018-05-18

Creating a User Account

You create a user account when you want a person to have access to the EcoStruxure BMS.

Visa mer
action_close

Using WebStation, you can create and administer user accounts.

You can also add a new user account to an already existing user group in the system. You can force users to change their password the next time they log on. Unused accounts can be disabled and saved for further use or they can be deleted from the system.

To create a user account
  1. In WebStation, click System .

  2. In the System pane, click Domains .

  3. In the Domains pane, click the domain where you want to create the user.

  4. Click Users .

  5. In the Users pane, click Add .

  6. In the User name box, type the user name.

  7. In the Password box, type the password.

  8. In the First name box, type the first name.

  9. In the Middle name box, type the middle name.

  10. In the Last name box, type the last name.

  11. In the Home email box, type the home email address.

  12. In the Work email box, type the work email address.

  13. In the Disable field, select True to disable the account.

  14. In the Force password change field, select True to force the user to change the password the next time the user logs on.

  15. In the Expiration box, enter the expiration date for the user account.

  16. In the Language list, select the language.

  17. In the Date, time and number format list, select the date, time and number format.

  18. In the System of measurement list, select the system of measurement.

  19. In the Member of box, select which user groups you want the user to be a member of.

  20. Click Save .

  • Create and Administer User Accounts in WebStation
  • Password Policy
  • Forcing Users to Change Their Passwords
  • Disabling a User Account
  • Deleting a User Account
  • Add and Edit User Dialog Box