earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: WebStation
Funktionaliteter: Användarhantering
Produktversion: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2018-05-18

Forcing Users to Change Their Passwords

You force users to change their passwords to strengthen the security in the system.

Visa mer
action_close

Using WebStation, you can create and administer user accounts.

You can also add a new user account to an already existing user group in the system. You can force users to change their password the next time they log on. Unused accounts can be disabled and saved for further use or they can be deleted from the system.

To force users to change their passwords
  1. In WebStation, click System .

  2. In the System pane, click Domains .

  3. In the Domains pane, click the domain where the user is located.

  4. Click Users .

  5. In the User s pane, click the user.

  6. In the Force password change box, select True .

  7. Click Save .

  • Create and Administer User Accounts in WebStation
  • Creating a User Account
  • Disabling a User Account
  • Deleting a User Account
  • Add and Edit User Dialog Box