Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2024, 7.0
03/12/2024

Editing a Backup Schedule

You edit a backup schedule, which is combined with a backup rule, to change the frequency of the backup. 

Afficher plus
action_close

The EcoStruxure Building Operation database includes a digital schedule that is combined with a default backup rule. Using this schedule and rule, the system automatically backs up all data on an EcoStruxure BMS server every Sunday at 01:00. You can edit the schedule settings for this backup rule, but you cannot delete the schedule and select another.

Pour plus d'informations, voir Editing a Backup Schedule .

Déclaration

If the automatically scheduled backup occurs during a Daylight Savings Time transition, the backup will not occur. To prevent loss of data, change the scheduled backup to a time that does not conflict with your region's Daylight Savings Time transition.

 
action_zoom_plus_stroke Backup on a standalone field server
Figure : Backup on a standalone field server

You can create a custom backup rule and then modify its schedule. For example, you can create a backup rule that backs up all data on a field server daily at 02:00.

Pour plus d'informations, voir Creating a Backup Rule .

To edit a backup schedule
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Backup rules .

  4. In the Backup Rules view, in the Schedule column, click the schedule that you want to modify.

  5. Revise the schedule and then click the Save button

     
    action_zoom_plus_stroke
    .

  • Backup Schedules
  • Backup Rules View
  • Adding a Weekly Event
  • Editing a Weekly Event
  • Adding a Date Exception Event
  • Editing a Date Exception Event
  • Adding a Date Range Exception Event
  • Editing a Date Range Exception Event
  • Adding a Calculated Exception Event
  • Editing a Calculated Exception Event
  • Schedule Editor ​– Basic View
  • Synchronizing EcoStruxure BMS Server Backups on a Network
  • Backup Rules View
  • Advanced Schedule Editor – Graphic View
  • Edit Time Value Period Dialog Box