Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2024, 7.0
02/12/2024

Synchronizing EcoStruxure BMS Server Backups on a Network

You synchronize all EcoStruxure BMS server backups to increase efficiency by centralizing the automated backup management on a single EcoStruxure BMS server, rather than across multiple EcoStruxure BMS servers.

Afficher plus
action_close

A synchronized backup is a method of performing a recurring, simultaneous backup of a selected number of EcoStruxure BMS servers. You can use a lead and shadow relationship to automate all the EcoStruxure BMS server backups on your network. Using this method, you configure and manage one lead backup rule on one EcoStruxure BMS server, which other backup rules can reference.

 
action_zoom_plus_stroke Synchronized recurring backup – Lead/Shadow method
Figure : Synchronized recurring backup – Lead/Shadow method

The system synchronizes all the shadow rules with the lead backup rule, and all the shadow schedules with the lead schedule. Pour plus d'informations, voir Synchronizing EcoStruxure BMS Server Backups on a Network .

To synchronize EcoStruxure BMS server backups on a network
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Backup Rules .

  4. In the Lead rule column, enter a backup rule that you want to use as the lead rule for one or more EcoStruxure BMS servers in the list.

    Déclaration

    When you select a lead rule, the backup rule on an EcoStruxure BMS server becomes a shadow of the lead rule.

  5. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Scheduled Backups
  • Synchronized Backups
  • Removing a Lead Rule from a Backup Rule
  • Editing a Backup Rule
  • Editing a Backup Schedule
  • Backup Rules View