You edit a calculated exception event to change the information about an exception event.
In WebStation, in the System Tree pane, select the schedule you want to edit.
In the Schedule workspace, navigate to the event you want to edit.
In the Event grid, click the calculated exception event you want to edit.
Edit the properties.
Component |
Description |
Event type |
Click Exception to display the exception types. |
Exception type |
Select Calculated for an exception type to apply the schedule. |
All Day |
Select All Day for an all day event. |
Start time |
Double-click and type a start time for the exception event. |
End time |
Double-click and type an end time for the exception event. |
Value |
Double-click and type a value for the exception event. |
Name |
Type a name for the event. |
Priority |
Select a priority number between 1 (highest priority) and 16 (lowest priority). |
Year |
Displays the current year, which is the default for the Calculated exception view. |
Month |
Select a month for the exception event or Odd month , Even month , Any month . |
Week of month |
Select a week of the month for the exception event or First , Second , Third , Fourth , Fifth , Last , Any week . |
Day of week |
Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting. |
Click Update .
To help you avoid mistakes, WebStation warns you when you make changes in a schedule or calendar for today’s date.