earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 1.8, 1.9
2015/5/22

Editing Registration Details

You must add your registration details before licenses can be activated. The registration details are written to the license details when a license is activated.

注释:
  • You need to enter the customer details before a licenses is activated.

  • Only English letters are allowed in the license details.

显示更多
action_close

The License Administrator administers the activation, return, and repair of licenses.

Registration Details

Before the first network license is activated on the License Server, details about the customer’s organization and the contact information of the account manager must be entered. The registration details are written to the license details when a license is activated. Building Operation automatically saves these registration details and reuses the details the next time a license is activated.

注释:

​Only English letters are allowed in the license details.

If you change the registration details, the changes are applied to all licenses located on the License Server.

注释:
  • To ensure that all the licenses have the same information, the registration details must be updated on all License Servers in the Building Operation system.

License Server Address

​During the installation of License Administrator on WorkStations or Enterprise Servers, you need to type the network address to the License Server where network licenses are available for check out. The address to the License Server can later be entered or edited through License Administrator or directly in the Windows registry ​of the computer or Enterprise Server that hosts the licensed product.

有关更多信息,请参阅 ​License Server Address .

To edit registration details
  1. In License Administrator, click the Registration Details view.

     
    action_zoom_plus_stroke
  2. In the License owner box, type the name of the organization that owns the license.

  3. In the Industry box, select the license owner’s field of business.

  4. In the Type of project boxes, select the proposed field of application for the license.

  5. In the Name box, type the name of the account manager that supplied the license.

  6. In the E-mail box, type the e-mail address to the account manager that supplied the license.

  7. In the Telephone number box, type the telephone number to the account manager that supplied the license.

     
    action_zoom_plus_stroke
  8. Click OK .

  9. Click Yes .

     
    action_zoom_plus_stroke

Any changes in the registration details updates all activated licenses on the License Server.

注释:
  • The customer details must be edited or updated individually on all License Servers.

  • Activating Network Licenses
  • License Administrator
  • Registration Details View