earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 2023
2022/12/17

Extended Trend Log Properties – Basic Tab

Use the Basic tab to configure the Extended trend log.

 
action_zoom_plus_stroke Extended Trend Log properties - Basic Tab
图: Extended Trend Log properties - Basic Tab

表格: Extended Trend Log Properties - Basic Tab

Component

Description

Monitored trend log

Enter the path to the trend log you want to transfer records from.

Unit

The unit of an extended trend log created from the trend log wizard at the same time as the connected trend log inherits the unit of measurement from the connected trend log.

The unit of an extended trend log that is manually connected to a trend log needs to be manually configured to use the same unit of measurement as the connected trend log.

Smart log

Select True to optimize the transfer of the monitored trend log to the extended trend log.

Threshold

Select the percentage threshold at which the trend log transfers its records to the extended trend log.

Maximum transfer interval

Select the maximum length of time that can pass between transfers from the monitored trend log to the extended trend log.

Transfer trigger variable

Enter a trigger variable to force a transfer of all records from the trend log to the extended trend log, for example, to generate a complete report.

有关更多信息,请参阅 扩展趋势日志 .

Log size

Select the number of records to store before old records are overwritten, including internal records generated by the trend log.

有关更多信息,请参阅 日志记录存储 .

Include in report s

Select True to include the extended trend log data in reports.

  • 扩展趋势日志
  • 配置对话框 – 操作标签
  • Configure Dialog Box – Configuration Tab
  • General Information Properties – Basic Tab
  • References Tab
  • Records Are Not Transferred to the Extended Trend Log