earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
9/4/2018

Viewing an Unforced Value

You view an unforced value of a forced value when you want to see the real value.

Show More
action_close

When you force a value, all input from the system is overridden. For example, a schedule is set to start a fan at 09:00 but you want it to start at 08:00. In this case, you can force the fan to start at 08:00.

You can manually release a forced value at any time or you can automate the release, using a Timed Force utility object to specify the duration or end time of the force. For more information, see Timed Force Objects .

When you release a forced value, the value returns to its normal status.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. For more information, see Viewing an Unforced Value .

Indication in WorkStation

A forced value is indicated by orange color in the properties dialog boxes. In in the Watch pane, a forced value is indicated by a pointing hand

 
action_zoom_plus_stroke
.

In the List View and Search View, a forced value is indicated by the text [Forced] in the 'Value' column.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. For more information, see Viewing an Unforced Value .

Indication in WebStation

A forced value is indicated by orange color and a pointing hand in the List view.

Indication in Function Block Graphics Viewer

A forced value is indicated by orange color in Function Block Graphics Viewer. For more information, see Forced Value Indication in Function Block Graphics Viewer .

To view an unforced value
  1. In WorkStation , in the System Tree pane, select the forced value.

  2. On the File menu, click Properties .

  3. Click Configure

     
    action_zoom_plus_stroke
    .

  4. Click the Operations tab.

  5. In the Unforced value box, view the unforced value.

  • Forced Values
  • Changing Value Dialog Box
  • Forcing a Value
  • Force and Unforce Buttons
  • Releasing a Forced Value
  • Searching for Forced Values