You can change and force values using a graphic or the Properties pane. Using the Watch pane, you can dynamically monitor a value.
When you force a value, all input from the system is overridden. For example, a schedule is set to start a fan at 09:00 but you want it to start at 08:00. In this case, you can force the fan to start at 08:00.
For more information, see Forced Values .
You can add or change units and prefixes on values using WebStation.
For more information, see Adding or Changing a Unit and Prefix for a Value in WebStation .