earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: WorkStation, WebStation
Funkcje: Harmonogramy
Wersja produktu: 2022, 2023
2024-11-25

How Schedules Work

Schedules are used to schedule the operation of parts of the BMS, such as a device or a setpoint. For example, a you can set up a schedule to make a device to operate between 08:00 and 17:00 every workday.

Schedules can be overridden by different types of exceptions. For example, if you want to shut down a device the last Friday in every month due to maintenance, you can use a calculated exception. The exception is added to the schedule and turns off the device the last Friday in every month.

If you want to shut down the device during the summer vacation, you can use a Calendar exception. In this case, you use an already created calendar that defines the summer vacation. This calendar is added to the schedule as an exception and the device will be shut down during all days of the summer vacation defined by the calendar.

Schedule Editor in WorkStation

 
action_zoom_plus_stroke Schedule editor calendar exceptions
Rysunek: Schedule editor calendar exceptions

The Basic view of the Schedule Editor serves as a workspace to plan and design a schedule. You use this editor to create, manage, and display weekly scheduled events and exception events.

Więcej informacji zawiera Basic View of the Schedule Editor .

Schedule Editor in WebStation

The Schedule Editor serves as a workspace to plan and design a schedule. You use this editor to create, manage, and display weekly scheduled events and exception events.

Więcej informacji zawiera Schedule Editor in WebStation .

Schedule Colors in WorkStation

A schedule has a color code so you can identify weekly events and exception events at a glance. This color code can assist you when you are modifying your schedule or trying to troubleshoot any problems.

Więcej informacji zawiera Schedule Colors in WorkStation .

Schedule Colors in WebStation

A schedule has a color code so you can identify weekly events and exception events at a glance. This color code can assist you when you are modifying your schedule or trying to troubleshoot any problems.

Więcej informacji zawiera Schedule Colors in WebStation .

Schedule Navigation in WorkStation

You can navigate in a schedule day-by-day, month-by-month, or year-by-year.

Więcej informacji zawiera Schedule Navigation in WorkStation .

Schedule Navigation in WebStation

You can navigate in a schedule day-by-day, month-by-month, or year-by-year.

Więcej informacji zawiera Schedule Workspace Toolbar .

Schedule Events

A schedule has two types of events: weekly events and exception events. Weekly events occur every week at specified times. Exception events occur when the schedule deviates from the weekly schedule, such as during holidays. Exception events override the weekly events when there is an overlap.

Więcej informacji zawiera Schedule Events .

Calendars in WorkStation

A calendar is a list of dates. The calendar provides the schedule with the dates when the exception events shall occur. To save time, you can reference a single calendar rather than entering several exception events in a schedule.

Więcej informacji zawiera Calendars in WorkStation .

Calendars in WebStation

A calendar is a list of dates. The calendar provides the schedule with the dates when the exception events shall occur. To save time, you can reference a single calendar rather than entering several exception events in a schedule.

Więcej informacji zawiera Calendars in WebStation .

Schedules Types

You can create three types of schedules: Digital, Multistate, or Analog. You create a digital schedule if the schedule needs to control a device with two output states, such as On or Off. You create a multistate schedule if the schedule needs to control a device that has output states based on multiple states, such as low, medium, or high. You create an analog schedule if the schedule controls a device that gauges the output in real numbers.

Więcej informacji zawiera Schedule Types .

Xenta Schedules in WebStation

Xenta Time Schedules and Xenta Central Time Schedules can be edited in WebStation. You can add, edit and delete weekly and exception events. You can assign and unassign lead Xenta central schedules. The Xenta Time Schedules and Xenta Central Time Schedules must be created using WorkStation.

Więcej informacji zawiera Xenta Schedules in WebStation .

Multi Schedule Viewer in WebStation

You can create a Multi schedule viewer in WebStation to edit and view a number of schedules at the same time.

Więcej informacji zawiera Multi Schedule Viewer .

  • WorkStation Overview
  • WebStation Overview
  • Basic View of the Schedule Editor
  • Schedule Editor in WebStation
  • Schedule Colors in WorkStation
  • Schedule Colors in WebStation
  • Schedule Navigation in WorkStation
  • Schedule Workspace Toolbar
  • Schedule Events
  • Calendars in WorkStation
  • Calendars in WebStation
  • Schedule Types
  • Xenta Schedules in WebStation
  • Multi Schedule Viewer