Productos eCommission SmartX Controllers, MP-C, MP-V, RP-C, SmartX Sensor
Funcionalidades: Ingeniería, Dispositivos SmartX IP Controller
Versión del producto: 2022, 2023, 2024, 7.0
10/09/2024

Cambiar el PIN del adaptador Bluetooth de SpaceLogic

Cambie el PIN del adaptador Bluetooth de SpaceLogic para mejorar la seguridad. El PIN del adaptador Bluetooth está diseñado para que, por defecto, sea 333666 y habría que cambiarlo a un código más seguro antes de realizar la puesta en marcha del dispositivo. Configure la contraseña del acceso al Bluetooth en el controlador RP.

Mostrar más
action_close

You enter a 6-digit PIN to configure the password for RP controller Bluetooth Low Energy (BLE) access. The default PIN for Bluetooth access is 333666 which you should change at first use. Changing the property and then saving your changes overwrites the default PIN, or any previously-set PIN. A factory reset returns the PIN to its default.

Aviso

POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY

Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.

Failure to follow these instructions can result in loss of data or equipment damage.

To change the RP controller Bluetooth 6-digit PIN
  1. In WorkStation, in the System Tree pane, expand the BACnet Interface and then select the IP network.

  2. Select the RP controller.

  3. Expand the device folder and click System .

  4. In the List view , click Settings.

  5. In the File menu, click Properties .

  6. In the Bluetooth pin box, enter a 6-digit numeric PIN.

    The PIN is validated, so you should ensure that it is 6 numeric characters only. Leading zeroes are permitted.

    For Cybersecurity purposes, the following criteria are applicable:

    • The number you enter does not display in the interface and no confirmation appears when you finish.

    • The PIN is automatically downloaded on hosting (that is, the EcoStruxure BMS database PIN overwrites the locally set PIN)

    Aviso

    You can mass configure the BLE 6-digit PIN for multiple RP controllers. Use the Search function in WorkStation to locate the controllers and then use the Settings object and its Bluetooth pin property to change them.

  7. Click Save .

Aviso

POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY

Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.

Failure to follow these instructions can result in loss of data or equipment damage.

Para cambiar el PIN del adaptador Bluetooth de SpaceLogic
  1. Conéctese al adaptador Para obtener más información, consulte Conectarse a un controlador mediante Bluetooth .

  2. En la página Gestión del dispositivo Bluetooth , en el campo del PIN, escriba el nuevo PIN y pulse en Actualizar .

  3. Su dispositivo móvil o portátil con Windows 10 le pide desvincular el adaptador. Pulse Permitir .

  4. La aplicación móvil Commission vuelve a la página Dispositivos Bluetooth . En el adaptador, pulse el botón LED para iniciar la vinculación.

  5. En la aplicación móvil Commission, seleccione el adaptador y pulse Conectar .

  6. En la página Gestión del dispositivo Bluetooth , seleccione Descubrir dispositivo .

  7. Su dispositivo móvil o portátil con Windows 10 le pide el PIN del adaptador. Introduzca el nuevo PIN y pulse Permitir .

  8. Su dispositivo móvil o portátil con Windows 10 indica que la vinculación se ha realizado correctamente. Pulse en Cerrar .

    Aviso

    Asegúrese de habilitar la propiedad Bus del sensor en el objeto de Configuración del controlador RP. De lo contrario, el adaptador Bluetooth no funcionará. Para obtener más información, consulte BACnet/IP Controller Settings Properties – Basic Tab .

Ha cambiado correctamente el PIN del adaptador y puede conectarlo a un controlador.

  • Adaptador Bluetooth SpaceLogic
  • Conectarse a un controlador con el adaptador SpaceLogic Bluetooth
  • BACnet/IP Controller Settings Properties – Basic Tab