earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: eCommission SmartX Controllers, MP-C, MP-V, RP-C, SmartX Sensor
功能: 工程, SmartX IP Controller 设备
产品版本: 3.1, 3.2
2020/2/12

更改 eCommission Bluetooth Adapter 的 PIN

您可更改 eCommission Adapter 的 PIN 以实现最佳安全实践。Bluetooth Adapter PIN 设计为 333666 的默认代码并应当更改至安全代码,然后再执行设备调试。您可以在 RP Series 控制器中配置蓝牙访问的密码。

显示更多
action_close

You enter a 6-digit PIN to configure the password for RP Series controller Bluetooth Low Energy (BLE) access. The default PIN for Bluetooth access is 333666 which you should change at first use. Changing the property and then saving your changes overwrites the default PIN, or any previously-set PIN. A factory reset returns the PIN to its default.

通知

POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY

Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.

Failure to follow these instructions can result in loss of data or equipment damage.

To change the RP Series controller Bluetooth 6-digit PIN
  1. In WorkStation, in the System Tree pane, expand the BACnet Interface and then select the IP network.

  2. Select the RP Series controller.

  3. Expand the device folder and click System .

  4. In the List view , click Settings.

  5. In the File menu, click Properties .

  6. In the Bluetooth pin box, enter a 6-digit numeric PIN.

    The PIN is validated, so you should ensure that it is 6 numeric characters only. Leading zeroes are permitted.

    For Cybersecurity purposes, the following criteria are applicable:

    • The number you enter does not display in the interface and no confirmation appears when you finish.

    • The PIN is automatically downloaded on hosting (that is, the EcoStruxure BMS database PIN overwrites the locally set PIN)

    提示:

    You can mass configure the BLE 6-digit PIN for multiple RP Series controllers. Use the Search function in WorkStation to locate the controllers and then use the Settings object and its Bluetooth pin property to change them.

  7. Click Save .

通知

系统可用性、完整性和机密性的潜在危害

第一次使用时更改默认密码有助于防止未经授权访问设备设置、控件和信息。

不遵照这些说明可导致数据丢失或设备损坏。

更改 eCommission Bluetooth Adapter 的 PIN
  1. 连接至 Adapter。 有关更多信息,请参阅 通过蓝牙连接至控制器 .

  2. 蓝牙设备管理 页面上的 PIN 字段,键入新的 PIN 并选择 更新

  3. 您的移动设备或 Windows 10 笔记本电脑提示您取消与 Adapter 的配对。选择 允许

  4. eCommission 应用程序返回至 蓝牙设备 页面。在 Adapter 上,按下 LED 按钮以发起配对。

  5. 在 eCommission 应用程序中选择 Adapter,然后选择 连接

  6. 蓝牙设备管理 页面,选择 发现设备

  7. 您的移动设备或 Windows 10 笔记本电脑提示您输入 Adapter PIN。输入新 PIN 并选择 允许

  8. 您的移动设备或 Windows 10 笔记本电脑指示配对成功。选择 关闭

    重要:

    请确保在 RP Series 控制器设置对象上启用 传感器总线 属性。否则,蓝牙适配器将无法工作。 有关更多信息,请参阅 SmartX IP Controller Settings Properties – Basic Tab .

您已成功更改 Adapter PIN 并且可连接至控制器。

  • eCommission 蓝牙适配器
  • 通过蓝牙适配器连接至控制器
  • SmartX IP Controller Settings Properties – Basic Tab