Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.
You download an Application Image that contains a Configuration Menu to a BACnet/IP controller to configure a device. Use this workflow to implement the Configuration Menu using the eCommission SmartX Controllers mobile application. Related information can be found in the section after the flowchart.
Pour plus d'informations, voir Configure Controllers with the Configuration Menu Workflow .
You download the Configuration Menu to the BACnet/IP controller to configure the device.
Pour plus d'informations, voir Téléchargement d'un menu Configuration sur un contrôleur BACnet/IP .
After downloading the configuration menu to the controller, you view and modify the device properties from the configuration menu to complete device commissioning.
Pour plus d'informations, voir Modification des propriétés du dispositif depuis le menu Configuration .