The License Administrator administers the activation, return, and repair of licenses.
During the installation of License Administrator on WorkStations or Enterprise Servers, you need to type the network address to the License Server where network licenses are available for check out. The address to the License Server can later be entered or edited through License Administrator or directly in the Windows registry of the computer or Enterprise Server that hosts the licensed product.
For more information, see License Server Address .