earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: ​License Administrator, ​License Server
Functionalities: License Management
Product version: 3.0, 3.1
11/30/2019

Licensing Overview

arrow1_rotationLicensing Model arrow1_rotationLicense System arrow1_rotationLicense Management arrow1_rotationService and Maintenance arrow1_rotationLicense Information arrow1_rotationDevice Administrator Licenses

The EcoStruxure Building Operation software is available for all to download and install. However, you need valid licenses to use the software. The number of users of the software is limited to the number of licenses owned by the customer.

Licensing Model

EcoStruxure BMS uses a license model that allows scalable pricing. An EcoStruxure BMS can be tailored with the features and size that is required by that solution. When setting up a new EcoStruxure BMS, consider the size, the extra features required, and the number of licenses to accommodate the size and features. The license policy lets you make an initial investment that corresponds to the required capacity and functionality at the beginning of the project and then allows for further investment in the future to expand the capacity or functionality.

For more information, see Licensing Model .

License System

​When setting up a new EcoStruxure BMS, you need to consider the size of the system, its structure, and the number of licenses to order and distribute.

For more information, see License System .

License Management

The EcoStruxure Building Operation license system consists of, for example, a License Server, WorkStation with client tools, and the Enterprise Server. The number of each component varies depending on the system size and architecture.

For more information, see License Management .

Service and Maintenance

The EcoStruxure Building Operation license policy is strictly controlled and is sensitive to any changes on the License Server, both hardware and software.

For more information, see Service and Maintenance .

License Information

The License Information in the Control Panel gives you an overview of the licenses in your EcoStruxure BMS.

For more information, see License Information .

Device Administrator Licenses

Device Administrator is used to manage licenses on SmartX server.

For more information, see Device Administrator Licenses .

  • Licensing, Installation, and Localization Overview
  • License System
  • License Management
  • Service and Maintenance
  • License Information
  • Device Administrator Licenses