earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 趋势
产品版本: 1.8
2016/10/13

Meter Trend Log Properties

Use the Meter Trend Log properties to configure the meter trend log.

 
action_zoom_plus_stroke Meter trend log properties
图: Meter trend log properties

表格: Meter Trend Log Properties

Component

Description

Status

​Displays the status of the trend log.

Enabled

​Displays True if the trend log is enabled.

Logged variable

Enter the variable that you want to log.

Delta

​Select the minimum value change that triggers a new record.

Trigger variable

Enter the variable that triggers the trend log to start recording.

Trigger condition

​Select when you want the variable recorded: when trigger variable changes to true, changes to false, or all changes. 有关更多信息,请参阅 Variable Triggered Trend Logs .

Log size

Select the number of records to store before old records are overwritten including internal records generated by the trend.

有关更多信息,请参阅 Log Record Storage .

Clear when enabled

​Select True to clear the trend log when it is enabled.

  • Trend Log Types
  • Meter Trend Logs
  • Configure Dialog Box – Configuration Tab
  • Configure Dialog Box – Operation Tab
  • Log Record Storage
  • Meter Trend Log Calculation Fails
  • Missing Trend Log Records
  • General Information Properties – Basic Tab
  • References Tab