earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 3.3, 2022
12/17/2021

Automation Server Replacement Using Restore Workflow

Use the workflow to duplicate the automation server from a backup set.

 
action_zoom_plus_stroke Duplicate automation server using restore flowchart
Figure: Duplicate automation server using restore flowchart
Copy automation server Backup Set to WorkStation

Save the most current backup set of the automation server that you want to replace to WorkStation.

For more information, see Saving an Automation Server Backup Set to Another Location .

Add new automation server to network and configure communication settings

Add the new automation server to the network and configure the IP address.

For more information, see Configuring an Automation Server to Use DHCP .

For more information, see Configuring the Automation Server IP Address .

Log on to automation server using WorkStation

For more information, see Logging on to WorkStation as an EcoStruxure Building Operation User .

Import backup set

Import the backup set to the new automation server.

For more information, see Importing a Backup Set to Automation Server .

Restore new automation server using the imported Backup Set

Restore the new automation server using the imported backup set.

For more information, see Restoring the EcoStruxure BMS Server .

Tip:

If the automation server does not go online, you can manually recreate the automation server or restore the connections between the Enterprise Server and the automation server. For more information, see Automation Server Remains Offline After Restore .

The Restore process automatically renames the automation server and specifies the objects and properties that the automation server uses to reestablish links and go online.

  • Restore
  • Automation Server Replacement Using Restore
  • Backup Sets
  • Saving an Automation Server Backup Set to Another Location
  • Configuring an Automation Server to Use DHCP
  • Configuring the Automation Server IP Address
  • Logging on to WorkStation as an EcoStruxure Building Operation User
  • Importing a Backup Set to Automation Server
  • Restoring the EcoStruxure BMS Server
  • Automation Server Remains Offline After Restore