earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 3.2, 3.3
4/27/2023

Restoring the EcoStruxure BMS Server

You restore the EcoStruxure BMS server to revert back to a previous snapshot of the EcoStruxure BMS server data.

Show More
action_close

Restore is the process of restoring data to an original or former state. Using Restore, you can revert to a previous snapshot of the EcoStruxure BMS server data despite any configuration changes made since the last backup. In the EcoStruxure BMS, Restore is a manual process designed to avoid the accidental overwriting of current EcoStruxure BMS server data.

Restored Data

Depending on what is contained in the backup file, you can restore different types of data.

  • Configuration only : the EcoStruxure Building Operation software restores the configuration database and custom object type data. Any existing historical data is lost when you select this option.

  • All data : the EcoStruxure Building Operation software restores the configuration, historical, and custom object types data.

For more information, see Restored Data .

Automation Server Replacement Using Restore

Backup and Restore helps assure that automation server data can be restored to a replacement automation server in the event of detected failure, or to the same automation server in the event of data loss. As a precaution, you back up your automation servers regularly so that you can use the most current backup to restore the automation server data to a replacement automation server. You also configure the new automation server to match the name and the network settings of the replaced automation server so the system can identify this automation server when online.

For more information, see Automation Server Replacement Using Restore .

Duplicate Automation Server Using Restore

You can use the Restore function to re-use the configuration data from a backup set in a new standalone automation server. Rather than manually configuring your preferred automation server configuration, you can save time and configure the standalone automation server from a backup set.

The backup set used can originate from an automation server that is or has been part of a multi-server configuration.

For more information, see Duplicate Automation Server from a Backup Set .

Important:

If your system includes the Reports Server and the Enterprise Server or Enterprise Central, stop the Reporting Agent service on the Reports Server first to prevent report generation during a restore of the Enterprise Server or Enterprise Central. For more information, see Stopping the Reporting Agent Windows Service .

To restore the EcoStruxure BMS server
  1. Stop the Reporting Agent service on the Reports Server. For more information, see Stopping the Reporting Agent Windows Service .

  2. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server that you want to restore.

  3. On the Actions menu, click Restore .

    Tip:

    Take manual control of any output points that could potentially damage equipment before restoring the EcoStruxure BMS server. If you cannot disconnect the physical outputs, restore the EcoStruxure BMS server using a trusted restore file that will turn off/on the outputs predictably and safely.

  4. In the Restore Options dialog box, in the Available restore points list, select a backup set in black text, which indicates that the backup set is compatible with the current version of the EcoStruxure BMS server.

  5. Select the type of data you want to restore:

    • Select Configuration only to restore only configuration and custom object types' data.

    • Select All data to restore the configuration, historical, and custom object types data.

  6. Click Restore .

  7. Click Yes .

  8. Click Close .

    If your system includes the Reports Server, the Reporting Agent Windows service restarts automatically.

  9. If you restore an Enterprise Central or an Enterprise Server that is not using the default ports, restart the server to restore the ports. For more information, see Restarting the Enterprise Server Windows Service .

  • Restore
  • Duplicate Automation Server from a Backup Set
  • Restore Options Dialog Box
  • Restoring an Automation Server from the Enterprise Server
  • Stopping the Reporting Agent Windows Service
  • Backup Set Text is Red
  • Restarting the Enterprise Server Windows Service