You restore the SmartStruxure server to revert back to a previous snapshot of the SmartStruxure server data.
If your system includes the Reports Server and the Enterprise Server, stop the Reporting Agent service on the Reports Server first to prevent report generation during a restore of the Enterprise Server. For more information, see Stopping the Reporting Agent Windows Service .
In WorkStation, in the System Tree pane, select the SmartStruxure server that you want to restore.
On the Actions menu, click Restore .
Take manual control of any output points that could potentially damage equipment before restoring the SmartStruxure server. If you cannot disconnect the physical outputs, restore the SmartStruxure server using a trusted restore file that will turn off/on the outputs predictably and safely.
In the Available restore points list, select a backup set in black text, which indicates that the backup set is compatible with the current version of the SmartStruxure server.
Select the type of data you want to restore:
Select Configuration only to restore only configuration and custom object types' data.
Select All data to restore the configuration, historical, and custom object types data.
Click Restore .
Click Yes .
Click Close .
If your system includes the Reports Server, the Reporting Agent Windows service restarts automatically.