earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, AS-P, WorkStation, Virtual Project Servers
Functionalities: Basic Functionality, Engineering
Product version: 1.8, 1.9
10/13/2016

Duplicate SmartStruxure Server Device from a Backup Set

You can use the Restore function to re-use the configuration data from a backup set in a new standalone SmartStruxure server device. Rather than manually configuring your preferred SmartStruxure server device configuration, you can save time and configure the standalone SmartStruxure server device from a backup set.

The backup set used can originate from a SmartStruxure server device that is or has been part of a multi-server configuration.

To store a backup set in another location, you save a selected backup set to a folder on your WorkStation PC or network drive.

For more information, see Backup Sets .

Protocol Compatibility

The restore function to re-use configuration data from a backup set is supported for all Building Operation supported protocols, except for BACnet and b3 BACnet.

LonWorks Devices Neuron IDs deleted on duplicated SmartStruxure server device

The LonWorks devices connected to the SmartStruxure server device are not the same as the LonWorks devices that are to be connected to the duplicate. When you create a duplicate from a SmartStruxure server device, all Neuron IDs in the duplicate are deleted. This is also a way to avoid network conflicts.

After you created the duplicate, you add new Neuron IDs to the duplicate. You then commission all LonWorks devices on the new SmartStruxure server device.

For more information, see LonWorks Device Workflows .

Password deleted on duplicated SmartStruxure device

When you duplicate a SmartStruxure device from a backup set all passwords are deleted on the duplicate for security reasons. The only exception is the default admin password. The administrator is forced to change the password at the first logon at the duplicate. All users must be given new passwords by the administrator.

Multi-server Site

To create a new SmartStruxure server device in a multi-server configuration, using a locally stored backup set, you need to make the backup set available for restore on the multi-server system. You add a new SmartStruxure server device to the Enterprise Server and select the backup set in the Create Object Wizard.

For more information, see Creating a SmartStruxure server device from a Backup Set .

Standalone SmartStruxure Server Device Site

You use a locally stored backup set to duplicate another SmartStruxure server device configuration in a standalone SmartStruxure server device. You then import the backup set to a client and restore to the new standalone SmartStruxure server device.

For more information, see Duplicating a SmartStruxure Server Device Using Restore  .

Duplicate SmartStruxure Server Device from a Backup Set Workflow

Use the following workflow to duplicate a SmartStruxure server device from a backup set.

 
action_zoom_plus_stroke Duplicate SmartStruxure server device using restore flowchart
Figure: Duplicate SmartStruxure server device using restore flowchart
Backup a SmartStruxure server device

Backup a SmartStruxure server device that has the configuration you want to use in the new standalone SmartStruxure server device.

For more information, see Backing Up SmartStruxure Servers Manually .

Copy backup set to local directory

Copy the backup set to a local directory.

For more information, see Saving a SmartStruxure Server Device Backup Set to Another Location .

Log on to standalone SmartStruxure server device

Log on to a new standalone SmartStruxure server device.

For more information, see Logging on to WorkStation as a Building Operation User .

Import backup set

Import the backup set.

For more information, see Importing a Backup Set to SmartStruxure Server Device .

Restore SmartStruxure server device using Restore configuration with new IDs

Use the Restore configuration with new IDs function to duplicate the configuration data from the imported backup set in the new standalone SmartStruxure server device. The communication settings from the backup set are not duplicated.

For more information, see Duplicating a SmartStruxure Server Device Using Restore  .

Important:

When you restore a standalone SmartStruxure server device, you are logged off and need to log on manually after the restore is complete.

  • Restore
  • Backup Sets
  • Creating a SmartStruxure server device from a Backup Set
  • Backing Up SmartStruxure Servers Manually
  • Saving a SmartStruxure Server Device Backup Set to Another Location
  • Logging on to WorkStation as a Building Operation User
  • Duplicating a SmartStruxure Server Device Using Restore 
  • LonWorks Device Workflows