earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2.0, 2.1, 3.0, 3.1
25/10/2018

Shortcut Presentation

Shortcuts without targets and shortcuts to objects are non-presentation objects. By default, non-presentation objects are not displayed in the System Tree, except when selected by means of the System Tree filter. However, a shortcut with an EcoStruxure BMS server or a folder as a target is a presentation object and is always displayed in the System Tree.

When a shortcut is created in an EcoStruxure BMS server or folder by means of the File-New submenu or the New-Shortcut command of the Context menu, the shortcut has no valid target. In this case, only the overlay icon (a small arrow in a square) is displayed (because no target type is assigned).

 
action_zoom_plus_stroke Example of a shortcut without an assigned target
Figure : Example of a shortcut without an assigned target

When a target is assigned, the overlay icon of the shortcut is added on top of the icon of the target. Pour plus d'informations, voir Shortcut Properties – Basic Tab .

The following figure is an example of a shortcut for an analog value in the System Tree:

 
action_zoom_plus_stroke Example of a shortcut to an analog value
Figure : Example of a shortcut to an analog value

When you click a shortcut, the address of the shortcut is displayed in the address bar and the name of the shortcut is displayed in the the tab of the shortcut window.

  • Function Overview
  • Shortcuts Overview
  • Viewing Shortcuts
  • Shortcuts Icon
  • Shortcut Properties – Basic Tab