earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Trends
Product version: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
4/21/2015

Trend Chart Series Menu

Use the Trend Chart Series menu to hide a series in the trend chart, to remove a series from the trend chart, change the settings for a series, and to view the properties for a series.

 
action_zoom_plus_stroke Trend chart series menu
Figure: Trend chart series menu

Table: Trend Chart Series Menu

Command

Description

Visible

Click (select or clear the check box) to show or hide the series in the trend chart.

Settings

Click to open the Trend Chart Settings dialog box, where you can change the settings for the series.

For more information, see Trend Chart Settings Dialog Box – Series Tab .

For more information, see Trend Chart Settings Dialog Box – Axis Tab .

Remove

Click to remove the series from the trend chart.

Properties

Click to open the Properties dialog box, where you can view the properties for the series.

  • Trend Chart Series in WebStation
  • Trend Chart Settings Dialog Box – Series Tab
  • Trend Chart Settings Dialog Box – Axis Tab