earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 趋势
产品版本: 1.8
2016/10/13

Create Trend Log Wizard – Configure Meter Trend Log Page

Use the Configure Meter Trend Log page to configure the settings of the meter trend log.

 
action_zoom_plus_stroke Configure Meter Trend Log page
图: Configure Meter Trend Log page

表格: Configure Meter Trend Log Page

Component

Description

Logged variable

Enter the variable that you want to log.

 
action_zoom_plus_stroke

Set unit

Click to open the Unit Selection dialog box where you select the unit. 有关更多信息,请参阅 Unit Selection Dialog Box .

Trigger variable

Enter the variable that triggers the trend log to start recording.

Trigger condition

​Select when you want the variable recorded: when trigger variable changes to true, changes to false, or all changes. 有关更多信息,请参阅 Variable Triggered Trend Logs .

Log size

Select the number of records to store before old records are overwritten including internal records generated by the trend.

Available trend storage

Displays the trend storage usage and the number of records left in the trend storage.

Clear when enabled

​Select True to clear the trend log when it is enabled.

  • Meter Trend Logs
  • Meter Trend Log Properties
  • Unit Selection Dialog Box
  • Trend Units
  • Variable Triggered Trend Logs
  • Log Record Storage
  • Create Object Wizard – Naming the Object Page