earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 1.9
10/12/2017

User Access to Shortcuts and Targets

The software permissions of a shortcut and its target object can be independently configured to enable control of user group accessibility.

Whenever these software permissions are set such that the user can see the target object by means of the shortcut, the user has the same read/write access to the shortcut as is set up for the target object.

The shortcut inherits all the commands of the target object type (but not all of these commands act upon the target object).

Inherited commands applied at the shortcut operate on either the shortcut itself, or on the target object, as listed in the following table:

Table: Inherited Command Application

Command applied at shortcut

Command operates on…

Delete

Shortcut

Copy

Shortcut

Move

Shortcut

Rename

Shortcut

Cut/Paste

Shortcut

Shortcut properties

Shortcut

Properties

Target

Open

Target

Add to Watch

Target

Trend commands

Target

Create Alarm

Target

  • Function Overview
  • Shortcuts Overview
  • Assigning Path Permissions to a User Account