You edit a calendar exception event to change the information about an exception event.
In WebStation, in the System Tree pane, select the schedule you want to edit.
In the Schedule workspace, navigate to the event you want to edit.
In the Event grid, click the calendar exception event you want to edit.
Edit the properties.
Component |
Description |
Event type |
Click Exception to display the exception types. |
Exception type |
Select Calendar to initiate a calendar reference. |
All Day |
Select All Day for an all day event. |
Start time |
Double-click and type a start time for the exception event. |
End time |
Double-click and type an end time for the exception event. |
Value |
Double-click and type a value for the exception event. |
Name |
Type a name for the event. |
Priority |
Select a priority number between 1 (highest priority) and 16 (lowest priority). |
Calendar |
Enter a calendar to reference. |
Click Update .
To help you avoid mistakes, WebStation warns you when you make changes in a schedule or calendar for today’s date.