earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Schedules
Product version: 1.8, 1.9
2/3/2014

Schedule Event Properties Dialog Box – Calendar Reference View

Use the Calendar Reference View in the Schedule Event Properties dialog box to reference a calendar to apply to your schedule.

 
action_zoom_plus_stroke Schedule event properties dialog box – Calendar reference view
Figure: Schedule event properties dialog box – Calendar reference view

Table: Schedule Event Properties Dialog Box – Calendar Reference View

Component

Description

Event type

Click Exception to display the exception types.

Exception type

Select Calendar to initiate a calendar reference.

All Day

Select All Day for an all day event.

Start time

Double-click and type a start time for the exception event.

End time

Double-click and type an end time for the exception event.

Value

Double-click and type a value for the exception event.

Name

Type a name for the event.

Priority

Select a priority number between 1 (highest priority) and 16 (lowest priority).

Calendar

Enter a calendar to reference.

  • Exception Events in WebStation
  • Calendars in WebStation
  • Schedule Event Properties Dialog Box – Weekly View
  • Schedule Event Properties Dialog Box – Single Date Exception View
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Schedule Event Properties Dialog Box – Calculated Exception View