earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: WebStation
Функции: Расписания
Версия продукта: 2024, 7.0
02.12.2024

Schedule Event Properties Dialog Box – Weekly View

Use the Weekly View in the Schedule Event Properties dialog box to create a new weekly event for an existing schedule.

 
action_zoom_plus_stroke Schedule event properties dialog box – Weekly view
Рисунок: Schedule event properties dialog box – Weekly view

Таблица: Schedule Event Properties Dialog Box – Weekly View

Component

Description

All Day

Select to create an all day event.

Value

Enter a value for the exception event.

At

Enter the start time for the exception event.

Until

Enter the end time for the exception event.

  • Weekly Events in WebStation
  • Schedule Event Properties Dialog Box – Single Date Exception View
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Schedule Event Properties Dialog Box – Calculated Exception View
  • Schedule Event Properties Dialog Box – Calendar Reference View