earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: WebStation
Функции: Расписания
Версия продукта: 2024, 7.0
02.12.2024

Schedule Event Properties Dialog Box – Calendar Reference View

Use the Calendar Reference View in the Schedule Event Properties dialog box to reference a calendar to apply to your schedule.

 
action_zoom_plus_stroke Schedule event properties dialog box – Calendar reference view
Рисунок: Schedule event properties dialog box – Calendar reference view

Таблица: Schedule Event Properties Dialog Box – Calendar Reference View

Component

Description

All Day

Select to create an all day event.

Value

Enter a value for the exception event.

At

Enter the start time for the exception event.

Until

Enter the end time for the exception event.

Exception name

Type a name for the event.

Exception priority

Select a priority number between 1 (highest priority) and 16 (lowest priority).

Event type

Select Calendar .

Value

Enter the calendar you want to use.

Open calendar

Click to open the selected calendar for viewing or editing.

  • Exception Events in WebStation
  • Calendars in WebStation
  • Schedule Event Properties Dialog Box – Weekly View
  • Schedule Event Properties Dialog Box – Single Date Exception View
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Schedule Event Properties Dialog Box – Calculated Exception View