earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: WebStation
Функции: Расписания
Версия продукта: 2024, 7.0
02.12.2024

Schedule Event Properties Dialog Box – Calculated Exception View

Use the Calculated Exception View in the Schedule Event Properties dialog box to schedule recurring exceptions.

 
action_zoom_plus_stroke Schedule event properties dialog box – Calculated exception view
Рисунок: Schedule event properties dialog box – Calculated exception view

Таблица: Schedule Event Properties Dialog Box – Calculated Exception View

Component

Description

All Day

Select to create an all day event.

Value

Enter a value for the exception event.

At

Enter the start time for the exception event.

Until

Enter the end time for the exception event.

Exception name

Type a name for the event.

Exception priority

Select a priority number between 1 (highest priority) and 16 (lowest priority).

Event type

Select Calculated .

Month

Enter the month when the calculated exception event occurs.

Day of month

Enter the day of month when the calculated exception event occurs.

Day of week

Enter the day of week when the calculated exception event occurs.

  • Exception Events in WebStation
  • Schedule Event Properties Dialog Box – Weekly View
  • Schedule Event Properties Dialog Box – Single Date Exception View
  • Schedule Event Properties Dialog Box – Date Range Exception View
  • Schedule Event Properties Dialog Box – Calendar Reference View