earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Schedules
Product version: 1.8, 1.9
2/3/2014

Schedule Event Properties Dialog Box – Date Range Exception View

Use the Date Range Exception View in the Schedule Event Properties dialog box to schedule a date range exception.

 
action_zoom_plus_stroke Schedule event properties dialog box – Date range exception view
Figure: Schedule event properties dialog box – Date range exception view

Table: Schedule Event Properties Dialog Box – Date Range Exception View

Component

Description

Event type

Click Exception to display the exception types.

Exception type

Select Date range for the exception to apply to the schedule.

All Day

Select All Day for an all day event.

Start time

Double-click and type a start time for the exception event.

End time

Double-click and type an end time for the exception event.

Value

Double-click and type a value for the exception event.

Name

Type a name for the event.

Priority

Select a priority number between 1 (highest priority) and 16 (lowest priority).

Year

Select a year. You can use Any year as a valid entry.

Month

Select a month for the exception event or Odd month , Even month , Any month .

Day of month

Select a value for the day of the month. You can use Any Day and Last Day as valid entries.

Day of week

Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting.

  • Exception Events in WebStation
  • Schedule Event Properties Dialog Box – Weekly View
  • Schedule Event Properties Dialog Box – Single Date Exception View
  • Schedule Event Properties Dialog Box – Calculated Exception View
  • Schedule Event Properties Dialog Box – Calendar Reference View