earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 2023
2022/12/17

Editing an Extended Trend Log to be Included in Reports

You edit extended trend logs to be included in reports if you want trend log data to appear in the reports.

To edit an extended trend log to be included in reports
  1. In WorkStation, in the System Tree pane, click the extended trend log you want to include in reports.

  2. In the Extended Trend Log properties, in the Include in Reports box, select True .

  3. Click the Save button

     
    action_zoom_plus_stroke
    .

The extended trend log is set up to be included in reports.

  • 配置扩展趋势日志
  • Extended Trend Log Properties – Basic Tab
  • 扩展趋势日志