earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 警报
产品版本: 1.8
2016/10/13

Create Variable Status Alarm Wizard – Alarm Trigger Page

Use the Alarm Trigger page to configure the trigger settings of the variable status alarm.

 
action_zoom_plus_stroke Variable status alarm trigger page
图: Variable status alarm trigger page

表格: Variable Status Alarm Trigger Page

Component

Description

Forced

Select to trigger the alarm when the monitored variable status is forced. 有关更多信息,请参阅 强制和取消强制按钮 .

Overridden

Select to trigger the alarm when the monitored variable status is overridden. 有关更多信息,请参阅 Output Override Status .

Monitored variable

​Enter the path to the variable that is monitored by the alarm.

Disable alarm

Select to disable the alarm, for example, before deployment.

Alarm delay

​Enter the time, in seconds, the alarm has to be within the reset criteria before the alarm state is changed from alarm to reset.

Reset delay

​Enter the time, in seconds, the alarm has to be within the alarm criteria before the alarm is triggered.

Shunt variable 1

​Enter the shunt variable that is used to enable or disable the alarm. 有关更多信息,请参阅 Shunt Variables .

Invert

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. 有关更多信息,请参阅 Shunt Variables .

Operator

Select AND or OR to add logic between the first and the second shunt variable. 有关更多信息,请参阅 Shunt Variables .

Shunt variable 2

​Enter the second shunt variable that is used to enable or disable the alarm. 有关更多信息,请参阅 Shunt Variables .

Invert

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. 有关更多信息,请参阅 Shunt Variables .

  • Create Alarm Wizard – Presentation Page
  • Create Alarm Wizard – User Action Page
  • Create Alarm Wizard – Attachment Page
  • Variable Status Alarm Properties – Basic Tab
  • Create Object Wizard – Naming the Object Page
  • Variable Status Alarms