The Energy Monitoring Calendar Consumption report displays daily energy consumption. A monthly thumbnail view of each day shows the consumption in a line graph view. You can zoom in on a specific day or select multiple days and see the days overlaid on each other. This report shows consumption trends, and is useful for identifying deviations and exceptions.
The following table shows the input parameters for the report.
Input Parameters |
Description |
Meter |
Specifies the meter or site included in the report. |
Calendar month |
Specifies the month to display on the report. Each day of the month is represented by a graph of that day’s energy consumption. |
Utility type |
Specifies the type of utility (gas, electricity, or meter). |