The Energy Monitoring Consumption report compares the energy consumption of one or more power meters with a target value. You can select a period or date range, as well as specific meters and buildings. The report compares the same or multiple meters over the same or different periods.
The following table shows the input parameters for the report.
Input Parameters |
Description |
Utility type |
Specifies the type of utility (gas, electricity, or meter).
|
Power meter |
Specifies the meter or site included in the report. |
Start report date/time |
Specifies the start date and time for reporting on the energy consumption. |
End report date/time |
Specifies the end date and time for reporting on the energy consumption. |
Date filter |
Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent. For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days. Select Fixed date if you entered a Start report date/time and an End report date/time . |
Group interval |
Specifies the time interval, such as daily, weekly, for organizing and displaying the energy consumption data. |
Consumption target |
Specifies a comparative value. When the report runs, the actual energy consumption units are compared to the target value. |