You update the eCommission Bluetooth Adapter firmware to improve adapter performance.
Connect to the Adapter. For more information, see Connecting to a Controller through Bluetooth .
In the Bluetooth Device Management page, select Update Adapter Firmware . If this button is read-only, the Adapter contains the latest firmware.
On the eCommission Bluetooth Adapter, press and hold the push button for 9 seconds. The LED displays the DFU mode flashing sequence. For more information, see Bluetooth LED Functionality . The eCommission SmartX Controllers mobile application displays the firmware upgrade progress.
When the firmware upgrade is complete, select Done .
Remove the Adapter from the SmartX Sensor.
Plug the Adapter back into the SmartX Sensor.
In the eCommission application, in the Bluetooth Devices page, select the Adapter and select Connect .
When you successfully connect to the Adapter, the firmware upgrade is complete.