Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
You search for forced values to determine if the system runs normally and to reset forced values. Manually overridden I/O points are not included in the search result.
In WorkStation, on the Toolbar, click the Search button
In the Search view, in the text box, type your search.
To search for all forced values, type '*'.
In the In folder box, enter the folder where you want to start the search.
Select Include subservers to include automation subservers in the search.
Only subservers running EcoStruxure Building Operation BMS version 1.5 or higher are included in the search.
Select Stop if more than 1000 results to limit the search to 1,000 results.
Select Forced values only to search for forced values that were forced from within the EcoStruxure BMS.
Select In device to include values forced from outside the EcoStruxure BMS in the search. For example, values forced on the device.
In the Select Types dialog box, in the Include types box, select object types to include in your search.
Click the Add type button
Click OK .
In the Select Conditions box, enter the search conditions that have to be met before a search result is displayed.
Click the Add condition button
Click OK .
Click the Search button
The forced values in the EcoStruxure BMS are displayed.