earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Device Administrator, FDP Server
Functionalities: Engineering, License Management
10/30/2025

EcoStruxure BMS Server Licensing on Servers not Connected to Internet Workflow

Use this workflow to assign and activate licenses on EcoStruxure BMS servers that are not connected to Internet and cannot access License Activation Server.

Note:

Do not use this workflow if you are on a semi online system where the EcoStruxure BMS servers are not connected to Internet, but the Device Administrator is connected to the Internet.

For more information, see Semi Online System .

You need one computer running Device Administrator that is connected to Internet.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Assign and activate licenses on EcoStruxure BMS servers without Internet access workflow
Figure: Assign and activate licenses on EcoStruxure BMS servers without Internet access workflow
Install certificates on the EcoStruxure BMS server

Install certificates if you use HTTPS for communication.

For more information, see Device Administrator Certificate Workflow .

Entitlements

Make sure that you have the Entitlements containing the licenses. You need the email with the entitlement during the process.

For more information, see Order Information Request .

Add an entitlement in Device Administrator

In Device Administrator, you add entitlements that contains products and licenses.

This is done so that you can view all licenses that are available to be assigned and then activated.

Make sure that you have the HTML entitlement certificate file or the entitlement ID available .

There are two different procedures to add and set up an entitlement:

Assign licenses to the EcoStruxure BMS server

Use the License Products available in the entitlements to assign License Features to the EcoStruxure BMS servers.

For more information, see Assigning Licenses .

Create the request files

Create request files with the licenses you want to activate.

You gather, and download, the license information from the EcoStruxure BMS servers. This information is used to identify the licenses that is to be activated from the License Activation Server.

For more information, see Creating the Request Files when Activating Licenses on EcoStruxure BMS Server not Connected to Internet .

Activate request files on License Activation Server to receive response files

Activate the request files on License Activation Server to receive response files.

This step must be done a computer that is connected to Internet and has access to License Activation Server.

For more information, see Activating Request Files to Receive Response Files .

Send response files to the EcoStruxure BMS server

Send the response files to the EcoStruxure BMS servers to complete the activation.

For more information, see Sending the Response Files to the EcoStruxure BMS Server when Activating Licenses .

Backup the EcoStruxure BMS server

After the licenses has been installed, make a backup of the EcoStruxure BMS server to make sure that you do not lose the licenses if any problems occur.

For more information, see Backup .

  • Activating Request Files to Receive Response Files
  • Creating the Request Files when Activating Licenses on EcoStruxure BMS Server not Connected to Internet
  • Activate Licenses Offline Dialog Box
  • Sending the Response Files to the EcoStruxure BMS Server when Activating Licenses
  • Backup
  • Assigning Licenses
  • EcoStruxure BMS Server Licensing on Servers not Connected to Internet Workflow
  • Centralized Licensing on EcoStruxure BMS Servers Connected to Internet Workflow