earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Semantic
12/2/2024

Uploading Ontologies

You upload ontologies on your system so that the correct ontologies are used on the semantic database.

Show More
action_close

Semantic is based on ontologies.

When you navigate a semantic database the Sparql queries that are used in navigation are executed on the semantic database. The results are then sent to Enterprise Server or Enterprise Central.

EcoStruxure Building Operation supports Brick ontology version 1.3.

Upload Ontologies

You can at any time upload an ontology from the EBO server to the semantic database. In some occasions you need to upload the ontologies from the Enterprise Server or Enterprise Central to the semantic database. This is done, for example, if you want to restore a semantic database. It is also done if you change the location of your semantic database from the default installation to another computer.

For more information, see Uploading Ontologies .

Enterprise server and Enterprise Central are delivered with the following ontologies. These are uploaded to the semantic database the first time you upload ontologies.

  • The default graph

  • https://brickschema.org/schema

  • https://w3id.org/se/building/extension

  • https://w3id.org/se/building/nsp

  • https://w3id.org/se/building/project

To upload ontologies
  1. In WorkStation open System .

  2. Right-click Semantic and click Upload ontologies .

  • Semantic Overview
  • Configure EcoStruxure Building Automation System to use Semantic Workflow
  • Configuring the Semantic Settings
  • Ontologies
  • Configuring Semantic Permissions
  • Uploading Ontologies